Hi,
These days I'm using the mobile APP Starter Pro to configure the CC3220SF Wi-Fi profile (adding the SSID and password)
II found that with the character % and + inside the password, the Wi-Fi commissioning always fail. I have done the tests also using the RESTFUL API call to add the Wi-Fi profiles, but late the device cannot with the Wi-Fi network.
Can you help me to clarify some points about this issue:
*. Is it possible that the CC3220SF uses some encoding (UTF-8) to store these passwords? The symbol % is for special use and doesn't represent the symbol %, then this issue is produced.
*. Is this an internal issue of CC3220SF (an issue inside the Service Pack, for example)? Then we cannot fix it using another way to send the password to the device.
Now I'm using the service pack of the version 3.14.
Thanks and regards,
Yong