Other Parts Discussed in Thread: UNIFLASH,
I am having the same issue that I believe other people have reported when using the MacOS and the UniFlash/dslite.sh. Is there a solution? Thanks in advance!
MacOS: Catalina 10.15.7
UniFlash: 6.1.0
% /Applications/ti_09_2020/uniflash_6.1.0/dslite.sh --mode cc32xx device info --port /dev/cu.usbserial-A50285BI
Executing the following command:
> ./SLImageCreator device info --port /dev/cu.usbserial-A50285BI
For more details and examples, please refer to the UniFlash Quick Start guide.
Config file (cfg.json) doesn't exist, using defaults
INFO:root:COM PORT /dev/cu.usbserial-A50285BI
INFO:slbootloader.slbootloader:Connecting to device
INFO:slbootloader.slbootloader:--- Please power off the device ---
Press ENTER to continue
INFO:slbootloader.slbootloader:Power off
INFO:slbootloader.slbootloader:Set break signal
Traceback (most recent call last):
File "SLImageCreator.py", line 5191, in <module>
File "SLImageCreator.py", line 5187, in main
File "SLImageCreator.py", line 5159, in cmdline
File "SLImageCreator.py", line 4785, in command_device_info
File "SLImageCreator.py", line 1569, in connect_device
File "slbootloader/slbootloader.py", line 432, in connect_with_reset
File "site-packages/serial/serialposix.py", line 548, in setBreak
IOError: [Errno 25] Inappropriate ioctl for device