Other Parts Discussed in Thread: CC3220S,
I don't understand the difference between between the CC3220S and the CC3220SF. As far as I was aware, the entire reason to use the SF over the S is because it has internal flash. However, I do not seem to be able to get the device to boot without connecting the External Flash (I removed the External Flash chip from the LAUNCHXL to test this). Can someone please explain why the CC3220SF has internal flash that can't be used for bootloading?