Hello,
Please image that nRESET is generated by connecting VBAT_RESET and VBAT1 (nRESET is generated internally) on CC3220MODA.
In case the ramping transition time of VBAT1 is very long (e.g. 10ms from 0V to 3.3V), the functionality of internal RC filter may not work normally, and then nRESET ramping time will be the same as the ramping of VBAT1 (the timing of both signals are simultaneous).
Although the nRESET signal should be low while supplies are ramping up, what happens in the above case?
Or, is there any transition time constraint of VBAT1?
Best Regards,
Nomo