This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

booting problem

Other Parts Discussed in Thread: SYSCONFIG, OMAP3530, ADS7846, WL1271

Hello all. Iam very new to the linux environment and now i have problems with the mistral board boot up.

here is the my          printenv

OMAP35X-Family-GP rev 2, CPU-OPP2 L3-165MHz
OMAP3 EVM board + LPDDR/NAND
In:    serial
Out:   serial
Err:   serial
Hit any key to stop autoboot:  0
OMAP3_EVM # printenv
baudrate=115200
bootdelay=6
ethaddr=00:50:C2:7E:90:FF
tftp_kernel=tftpboot 0x80000000 uImage.499
bootargs_nfs=mem=88M console=ttyS0,115200n8 noinitrd itch the display from LCD to DVI during run time. This
netmask=255.255.255.0
ipaddr=192.168.0.167
serverip=192.168.0.150
bootfile=uImage.499
bootcmd=tftp 0x80000000 uImage.500;bootm
myip=192.168.0.167
tftpip=192.168.0.150
nfshost=192.168.0.150
bootserver=192.168.0.150
gatewayip=192.168.0.150
bootargs=console=ttyS0,115200n8 noinitrd ip=192.168.0.150 root=/dev/nfs rw nfsroot=SERVER:192.168.0.150, size=1024 mem=128M
stdin=serial
stdout=serial
stderr=serial

 

 

here is the booting process

<6>OMAP DMA hardware revision 4.0
<3>USB: No board-specific platform config found
<6>OMAP DSS rev 2.0
<6>OMAP DISPC rev 3.0
<6>OMAP VENC rev 2
<6>OMAP DSI rev 1.0
bio: create slab <bio-0> at 0
<6>i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
<6>twl4030: PIH (irq 7) chaining IRQs 368..375
<6>twl4030: power (irq 373) chaining IRQs 376..383
<6>twl4030: gpio (irq 368) chaining IRQs 384..401
<6>i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
<6>i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
<5>SCSI subsystem initialized
<6>usbcore: registered new interface driver usbfs
<6>usbcore: registered new interface driver hub
<6>usbcore: registered new device driver usb
<6>musb_hdrc: version 6.0, musb-dma, host, debug=0
<7>HS USB OTG: revision 0x33, sysconfig 0x2011, sysstatus 0x1, intrfsel 0x1, simenable  0x0
<7>musb_hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine (X), bulk split (X), HB-ISO Rx (X), HB-ISO Tx (X), SoftConn)
<7>musb_hdrc: MHDRC RTL version 1.400
<7>musb_hdrc: setup fifo_mode 4
<7>musb_hdrc: 29/31 max ep, 16384/16384 memory
<7>musb_hdrc: hw_ep 0shared, max 64
<7>musb_hdrc: hw_ep 1tx, max 512
<7>musb_hdrc: hw_ep 1rx, max 512
<7>musb_hdrc: hw_ep 2tx, max 512
<7>musb_hdrc: hw_ep 2rx, max 512
<7>musb_hdrc: hw_ep 3tx, max 512
<7>musb_hdrc: hw_ep 3rx, max 512
<7>musb_hdrc: hw_ep 4tx, max 512
<7>musb_hdrc: hw_ep 4rx, max 512
<7>musb_hdrc: hw_ep 5tx, max 512
<7>musb_hdrc: hw_ep 5rx, max 512
<7>musb_hdrc: hw_ep 6tx, max 512
<7>musb_hdrc: hw_ep 6rx, max 512
<7>musb_hdrc: hw_ep 7tx, max 512
<7>musb_hdrc: hw_ep 7rx, max 512
<7>musb_hdrc: hw_ep 8tx, max 512
<7>musb_hdrc: hw_ep 8rx, max 64
<7>musb_hdrc: hw_ep 9tx, max 512
<7>musb_hdrc: hw_ep 9rx, max 64
<7>musb_hdrc: hw_ep 10tx, max 512
<7>musb_hdrc: hw_ep 10rx, max 64
<7>musb_hdrc: hw_ep 11tx, max 256
<7>musb_hdrc: hw_ep 11rx, max 256
<7>musb_hdrc: hw_ep 12tx, max 256
<7>musb_hdrc: hw_ep 12rx, max 256
<7>musb_hdrc: hw_ep 13tx, max 256
<7>musb_hdrc: hw_ep 13rx, max 4096
<7>musb_hdrc: hw_ep 14shared, max 1024
<7>musb_hdrc: hw_ep 15shared, max 1024
<6>musb_hdrc: USB Host mode controller at d80ab000 using DMA, IRQ 92
<6>musb_hdrc musb_hdrc: MUSB HDRC host driver
<6>musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
<6>usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
<6>usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
<6>usb usb1: Product: MUSB HDRC host driver
<6>usb usb1: Manufacturer: Linux 2.6.29-rc3-omap1 musb-hcd
<6>usb usb1: SerialNumber: musb_hdrc
<6>usb usb1: configuration #1 chosen from 1 choice
<6>hub 1-0:1.0: USB hub found
<6>hub 1-0:1.0: 1 port detected
<7>Registered /proc/driver/musb_hdrc
<6>NET: Registered protocol family 2
<7>Switched to high resolution mode on CPU 0
<6>IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
<6>TCP established hash table entries: 4096 (order: 3, 32768 bytes)
<6>TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
<6>TCP: Hash tables configured (established 4096 bind 4096)
<6>TCP reno registered
<6>NET: Registered protocol family 1
<6>OMAP35x Linux PSP version 02.01.03.11 (OMAP3EVM)
<4>NetWinder Floating Point Emulator V0.97 (double precision)
<5>VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
<6>JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
<6>msgmni has been set to 245
<6>alg: No test for stdrng (krng)
<6>io scheduler noop registered
<6>io scheduler anticipatory registered (default)
<6>io scheduler deadline registered
<6>io scheduler cfq registered
Generic Backlight Driver Initialized.
<6>Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
<6>serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
<6>console [ttyS0] enabled
Linux version 2.6.29-rc3-omap1 (x0029463@psplinux050) (gcc version 4.2.3 (Sourcery G++ Lite 2008q1-126)) #1 Mon Sep 14 13:51:49 IST 2009
CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c5387f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: OMAP3 EVM
Memory policy: ECC disabled, Data cache writeback
OMAP3530 ES3.1 (full speed SGX, IVA2)
SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 32512
Kernel command line: console=ttyS0,115200n8 noinitrd ip=192.168.0.150 root=/dev/nfs rw nfsroot=SERVER:192.168.0.150, size=1024 mem=128M
Clocking rate (Crystal/DPLL/MPU core): 26.0/332/500 MHz
IVA2 clocking rate: 360 MHz
Reprogramming SDRC
GPMC revision 5.0
IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts
Total of 96 interrupts on 1 active controller
OMAP34xx GPIO hardware version 2.5
PID hash table entries: 512 (order: 9, 2048 bytes)
OMAP clockevent source: GPTIMER1 at 32768 Hz
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 125296KB available (3928K code, 370K data, 156K init)
Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
net_namespace: 520 bytes
NET: Registered protocol family 16
MUX: setup AF26_34XX_GPIO0 (0xd80021e0): 0x011c -> 0x0118
MUX: setup L8_34XX_GPIO63 (0xd80020ce): 0x0118 -> 0x0004
MUX: setup AF9_34XX_GPIO22 (0xd80025ec): 0x0100 -> 0x011c
MUX: setup U3_34XX_GPIO61 (0xd80020c8): 0x0118 -> 0x011c
MUX: setup AH14_34XX_GPIO21 (0xd80025ea): 0x0100 -> 0x011c
MUX: setup AA10_3430_USB2HS_PHY_STP (0xd80025f2): 0x0100 -> 0x0003
MUX: setup AA8_3430_USB2HS_PHY_CLK (0xd80025f0): 0x0100 -> 0x0003
MUX: setup AA9_3430_USB2HS_PHY_DIR (0xd80025f4): 0x0100 -> 0x010b
MUX: setup AB11_3430_USB2HS_PHY_NXT (0xd80025f6): 0x0100 -> 0x010b
MUX: setup AB10_3430_USB2HS_PHY_D0 (0xd80025f8): 0x0100 -> 0x010b
MUX: setup AB9_3430_USB2HS_PHY_D1 (0xd80025fa): 0x0100 -> 0x010b
MUX: setup W3_3430_USB2HS_PHY_D2 (0xd80021d4): 0x0108 -> 0x010b
MUX: setup T4_3430_USB2HS_PHY_D3 (0xd80021de): 0x0108 -> 0x010b
MUX: setup T3_3430_USB2HS_PHY_D4 (0xd80021d8): 0x0100 -> 0x010b
MUX: setup R3_3430_USB2HS_PHY_D5 (0xd80021da): 0x0100 -> 0x010b
MUX: setup R4_3430_USB2HS_PHY_D6 (0xd80021dc): 0x0108 -> 0x010b
MUX: setup T2_3430_USB2HS_PHY_D7 (0xd80021d6): 0x0100 -> 0x010b
twl4030: client 1 is not initialized
twl4030: client 1 is not initialized
MUX: setup AA21_34XX_GPIO157 (0xd800218e): 0x0018 -> 0x011c
MUX: setup C23_34XX_GPIO98 (0xd8002114): 0x0004 -> 0x011c
omap3evmdc: Driver registration complete
OMAP DMA hardware revision 4.0
USB: No board-specific platform config found
OMAP DSS rev 2.0
OMAP DISPC rev 3.0
OMAP VENC rev 2
OMAP DSI rev 1.0
bio: create slab <bio-0> at 0
i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
twl4030: PIH (irq 7) chaining IRQs 368..375
twl4030: power (irq 373) chaining IRQs 376..383
twl4030: gpio (irq 368) chaining IRQs 384..401
i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
musb_hdrc: version 6.0, musb-dma, host, debug=0
musb_hdrc: USB Host mode controller at d80ab000 using DMA, IRQ 92
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.29-rc3-omap1 musb-hcd
usb usb1: SerialNumber: musb_hdrc
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
NET: Registered protocol family 1
OMAP35x Linux PSP version 02.01.03.11 (OMAP3EVM)
NetWinder Floating Point Emulator V0.97 (double precision)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 245
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler anticipatory registered (default)
io scheduler deadline registered
io scheduler cfq registered
Generic Backlight Driver Initialized.
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
console [ttyS0] enabled
<6>serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
<6>serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
<6>brd: module loaded
brd: module loaded
<6>loop: module loaded
loop: module loaded
<6>smsc911x: Driver version 2008-10-21.
smsc911x: Driver version 2008-10-21.
<6>smsc911x-mdio: probed
smsc911x-mdio: probed
<6>eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:01, irq=-1)
eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:01, irq=-1)
<6>net eth0: MAC Address: 00:50:c2:7e:90:ff
net eth0: MAC Address: 00:50:c2:7e:90:ff
<6>Linux video capture interface: v2.00
Linux video capture interface: v2.00
<6>usbcore: registered new interface driver uvcvideo
usbcore: registered new interface driver uvcvideo
<6>USB Video Class driver (v0.1.0)
USB Video Class driver (v0.1.0)
<6>i2c /dev entries driver
i2c /dev entries driver
<4>Driver 'sd' needs updating - please use bus_type methods
Driver 'sd' needs updating - please use bus_type methods
<6>omap2-nand driver initializing
omap2-nand driver initializing
<6>NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)
<5>Creating 5 MTD partitions on "omap2-nand.0":
Creating 5 MTD partitions on "omap2-nand.0":
<5>0x000000000000-0x000000080000 : "xloader-nand"
0x000000000000-0x000000080000 : "xloader-nand"
<5>0x000000080000-0x000000240000 : "uboot-nand"
0x000000080000-0x000000240000 : "uboot-nand"
<5>0x000000240000-0x000000280000 : "params-nand"
0x000000240000-0x000000280000 : "params-nand"
<5>0x000000280000-0x000000780000 : "linux-nand"
0x000000280000-0x000000780000 : "linux-nand"
<5>0x000000780000-0x000010000000 : "jffs2-nand"
0x000000780000-0x000010000000 : "jffs2-nand"
<6>OneNAND driver initializing
OneNAND driver initializing
<6>ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
<6>ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
<6>ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 2
ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 2
<6>ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
<6>ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
<6>usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
<6>usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
<6>usb usb2: Product: OMAP-EHCI Host Controller
usb usb2: Product: OMAP-EHCI Host Controller
<6>usb usb2: Manufacturer: Linux 2.6.29-rc3-omap1 ehci_hcd
usb usb2: Manufacturer: Linux 2.6.29-rc3-omap1 ehci_hcd
<6>usb usb2: SerialNumber: ehci-omap.0
usb usb2: SerialNumber: ehci-omap.0
<6>usb usb2: configuration #1 chosen from 1 choice
usb usb2: configuration #1 chosen from 1 choice
<6>hub 2-0:1.0: USB hub found
hub 2-0:1.0: USB hub found
<6>hub 2-0:1.0: 3 ports detected
hub 2-0:1.0: 3 ports detected
<6>Initializing USB Mass Storage driver...
Initializing USB Mass Storage driver...
<6>usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb-storage
<6>USB Mass Storage support registered.
USB Mass Storage support registered.
<6>input: omap_twl4030keypad as /class/input/input0
input: omap_twl4030keypad as /class/input/input0
<6>ads7846 spi1.0: touchscreen, irq 335
ads7846 spi1.0: touchscreen, irq 335
<6>input: ADS784x Touchscreen as /class/input/input1
input: ADS784x Touchscreen as /class/input/input1
<6>OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
<6>cpuidle: using governor ladder
cpuidle: using governor ladder
<6>cpuidle: using governor menu
cpuidle: using governor menu
<6>usbcore: registered new interface driver usbhid
usbcore: registered new interface driver usbhid
<6>usbhid: v2.6:USB HID core driver
usbhid: v2.6:USB HID core driver
<6>Advanced Linux Sound Architecture Driver Version 1.0.19.
Advanced Linux Sound Architecture Driver Version 1.0.19.
<6>usbcore: registered new interface driver snd-usb-audio
usbcore: registered new interface driver snd-usb-audio
<4>No device for DAI twl4030
No device for DAI twl4030
<4>No device for DAI twl4030 Voice
No device for DAI twl4030 Voice
<4>No device for DAI omap-mcbsp-dai-0
No device for DAI omap-mcbsp-dai-0
<4>No device for DAI omap-mcbsp-dai-1
No device for DAI omap-mcbsp-dai-1
<4>No device for DAI omap-mcbsp-dai-2
No device for DAI omap-mcbsp-dai-2
<4>No device for DAI omap-mcbsp-dai-3
No device for DAI omap-mcbsp-dai-3
<4>No device for DAI omap-mcbsp-dai-4
No device for DAI omap-mcbsp-dai-4
<6>OMAP3 EVM SoC init
OMAP3 EVM SoC init
<6>TWL4030 Audio Codec init
TWL4030 Audio Codec init
<6>asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
<6>ALSA device list:
ALSA device list:
<6>  #0: omap3evm (twl4030)
  #0: omap3evm (twl4030)
<6>TCP cubic registered
TCP cubic registered
<6>NET: Registered protocol family 17
NET: Registered protocol family 17
<6>NET: Registered protocol family 15
NET: Registered protocol family 15
<6>RPC: Registered udp transport module.
RPC: Registered udp transport module.
<6>RPC: Registered tcp transport module.
RPC: Registered tcp transport module.
<3>Power Management for TI OMAP3.
Power Management for TI OMAP3.
<6>SmartReflex driver initialized
SmartReflex driver initialized
<6>Disabling unused clock "sr2_fck"
Disabling unused clock "sr2_fck"
<6>Disabling unused clock "sr1_fck"
Disabling unused clock "sr1_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "gpt2_ick"
Disabling unused clock "gpt2_ick"
<6>Disabling unused clock "gpt3_ick"
Disabling unused clock "gpt3_ick"
<6>Disabling unused clock "gpt4_ick"
Disabling unused clock "gpt4_ick"
<6>Disabling unused clock "gpt5_ick"
Disabling unused clock "gpt5_ick"
<6>Disabling unused clock "gpt6_ick"
Disabling unused clock "gpt6_ick"
<6>Disabling unused clock "gpt7_ick"
Disabling unused clock "gpt7_ick"
<6>Disabling unused clock "gpt8_ick"
Disabling unused clock "gpt8_ick"
<6>Disabling unused clock "gpt9_ick"
Disabling unused clock "gpt9_ick"
<6>Disabling unused clock "wdt3_ick"
Disabling unused clock "wdt3_ick"
<6>Disabling unused clock "wdt3_fck"
Disabling unused clock "wdt3_fck"
<6>Disabling unused clock "gpio2_dbck"
Disabling unused clock "gpio2_dbck"
<6>Disabling unused clock "gpio3_dbck"
Disabling unused clock "gpio3_dbck"
<6>Disabling unused clock "gpio4_dbck"
Disabling unused clock "gpio4_dbck"
<6>Disabling unused clock "gpio5_dbck"
Disabling unused clock "gpio5_dbck"
<6>Disabling unused clock "gpt9_fck"
Disabling unused clock "gpt9_fck"
<6>Disabling unused clock "gpt8_fck"
Disabling unused clock "gpt8_fck"
<6>Disabling unused clock "gpt7_fck"
Disabling unused clock "gpt7_fck"
<6>Disabling unused clock "gpt6_fck"
Disabling unused clock "gpt6_fck"
<6>Disabling unused clock "gpt5_fck"
Disabling unused clock "gpt5_fck"
<6>Disabling unused clock "gpt4_fck"
Disabling unused clock "gpt4_fck"
<6>Disabling unused clock "gpt3_fck"
Disabling unused clock "gpt3_fck"
<6>Disabling unused clock "gpt2_fck"
Disabling unused clock "gpt2_fck"
<6>Disabling unused clock "gpt12_ick"
Disabling unused clock "gpt12_ick"
<6>Disabling unused clock "wdt1_ick"
Disabling unused clock "wdt1_ick"
<6>Disabling unused clock "wdt2_ick"
Disabling unused clock "wdt2_ick"
<6>Disabling unused clock "wdt2_fck"
Disabling unused clock "wdt2_fck"
<6>Disabling unused clock "gpio1_dbck"
Disabling unused clock "gpio1_dbck"
<6>Disabling unused clock "des1_ick"
Disabling unused clock "des1_ick"
<6>Disabling unused clock "sha11_ick"
Disabling unused clock "sha11_ick"
<6>Disabling unused clock "rng_ick"
Disabling unused clock "rng_ick"
<6>Disabling unused clock "aes1_ick"
Disabling unused clock "aes1_ick"
<6>Disabling unused clock "ssi_ick"
Disabling unused clock "ssi_ick"
<6>Disabling unused clock "mailboxes_ick"
Disabling unused clock "mailboxes_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "gpt10_ick"
Disabling unused clock "gpt10_ick"
<6>Disabling unused clock "gpt11_ick"
Disabling unused clock "gpt11_ick"
<6>Disabling unused clock "hdq_ick"
Disabling unused clock "hdq_ick"
<6>Disabling unused clock "mspro_ick"
Disabling unused clock "mspro_ick"
<6>Disabling unused clock "des2_ick"
Disabling unused clock "des2_ick"
<6>Disabling unused clock "sha12_ick"
Disabling unused clock "sha12_ick"
<6>Disabling unused clock "aes2_ick"
Disabling unused clock "aes2_ick"
<6>Disabling unused clock "icr_ick"
Disabling unused clock "icr_ick"
<6>Disabling unused clock "pka_ick"
Disabling unused clock "pka_ick"
<6>Disabling unused clock "ssi_ssr_fck"
Disabling unused clock "ssi_ssr_fck"
<6>Disabling unused clock "hdq_fck"
Disabling unused clock "hdq_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mspro_fck"
Disabling unused clock "mspro_fck"
<6>Disabling unused clock "gpt11_fck"
Disabling unused clock "gpt11_fck"
<6>Disabling unused clock "sad2d_ick"
Disabling unused clock "sad2d_ick"
<6>Disabling unused clock "dpll4_m6x2_ck"
Disabling unused clock "dpll4_m6x2_ck"
<6>Disabling unused clock "dpll3_m3x2_ck"
Disabling unused clock "dpll3_m3x2_ck"
<6>VFP support v0.3: VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
implementor 41 architecture 3 part 30 variant c rev 1
<4>GPIO-153 autorequested
GPIO-153 autorequested
<3>omap-dss DISPC error: Requested pixel clock not possible with the current OMAP2_DSS_MIN_FCK_PER_PCK setting. Turning the constraint off.
omap-dss DISPC error: Requested pixel clock not possible with the current OMAP2_DSS_MIN_FCK_PER_PCK setting. Turning the constraint off.
<4>omap-dss: Could not find exact pixel clock. Requested 25190 kHz, got 25189 kHz
omap-dss: Could not find exact pixel clock. Requested 25190 kHz, got 25189 kHz
<4>Display already enabled
Display already enabled
<4>Display already enabled
Display already enabled
<6>Buffer Size = 3686400
Buffer Size = 3686400
<6>omap_vout: registered and initialized                        video device 0 [v4l2]
omap_vout: registered and initialized                   video device 0 [v4l2]
<6>Buffer Size = 3686400
Buffer Size = 3686400
<6>omap_vout: registered and initialized                        video device 1 [v4l2]
omap_vout: registered and initialized                   video device 1 [v4l2]
<6>display->updated
display->updated
<6>net eth0: SMSC911x/921x identified at 0xc885c000, IRQ: 336
net eth0: SMSC911x/921x identified at 0xc885c000, IRQ: 336
<5>Sending DHCP and RARP requests .Sending DHCP and RARP requests ........... timed out!
 timed out!
<3>IP-Config: Retrying forever (NFS root)...
IP-Config: Retrying forever (NFS root)...
<6>net eth0: SMSC911x/921x identified at 0xc885c000, IRQ: 336
net eth0: SMSC911x/921x identified at 0xc885c000, IRQ: 336
<5>Sending DHCP and RARP requests .Sending DHCP and RARP requests ...,, OK
 OK
IP-Config: Got DHCP answer from 192.168.0.5, IP-Config: Got DHCP answer from 192.168.0.5, my address is 192.168.0.167
my address is 192.168.0.167
IP-Config: Complete:IP-Config: Complete:
     device=eth0
     device=eth0, addr=192.168.0.167, addr=192.168.0.167, mask=255.255.255.0, mask=255.255.255.0, gw=192.168.0.1, gw=192.168.0.1,
     host=192.168.0.167, domain=nomor.local, nis-domain=(none),
     host=192.168.0.167, domain=nomor.local, nis-domain=(none),
     bootserver=192.168.0.5,
     bootserver=192.168.0.5, rootserver=192.168.0.5, rootserver=192.168.0.5, rootpath=/usr/lib/corebiz/nfsroot, rootpath=/usr/lib/corebiz/nfsroot

<5>Looking up port of RPC 100003/2 on 192.168.0.5
Looking up port of RPC 100003/2 on 192.168.0.5
<5>Looking up port of RPC 100005/1 on 192.168.0.5
Looking up port of RPC 100005/1 on 192.168.0.5
<3>Root-NFS: Server returned error -13 while mounting /tftpboot/SERVER:192.168.0.150
Root-NFS: Server returned error -13 while mounting /tftpboot/SERVER:192.168.0.150
<3>VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
Please append a correct "root=" boot option; here are the available partitions:
1f00             512 mtdblock01f00             512 mtdblock0 (driver?)
 (driver?)
1f01            1792 mtdblock11f01            1792 mtdblock1 (driver?)
 (driver?)
1f02             256 mtdblock21f02             256 mtdblock2 (driver?)
 (driver?)
1f03            5120 mtdblock31f03            5120 mtdblock3 (driver?)
 (driver?)
1f04          254464 mtdblock41f04          254464 mtdblock4 (driver?)
 (driver?)
<0>Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

Someone please  let me know what i have to do now

  • Hi Suresh,

    From the log it looks like you are using the OMAP35x- EVM and trying to boot the board from tftpboot and file system is on NFS server.

    In this forum we support the WL1271 based WLAN and WLAN+BT applications using OMAP35x/AM37x - GA releases (http://processors.wiki.ti.com/index.php/ARM_Processor_Wireless_Connectivity_Downloads). Those applications have been tested with jffs2 file system flashed into the NAND (Booting instructions are available in http://processors.wiki.ti.com/index.php/OMAP35x_Wireless_Connectivity_Getting_Started_Guide ) 

    If you want to use the EVM for some other purpose and need NFS file system, please post your queries on omap35x forum (http://e2e.ti.com/support/dsp/omap_applications_processors/f/447.aspx)

    Also you can try instructions in the wiki (http://processors.wiki.ti.com/index.php/AM35x-OMAP35x-PSP_03.00.00.05_UserGuide#Booting_Linux_Kernel)

    Thanks,

    Sinoj

     

     

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • Suresh,

    I see a couple of small problems with your definition of the parameter "nfsroot" in u-boot.  The definition of the parameter "nfsroot" should be the IP address of the NFS server followed by a colon and then the path to the NFS mount point in the server.  See example below and notice that there are no spaces in the definition of "nfspath".  I see a space in your definition of nfsroot after the comma.

    serverip=192.168.0.150
    nfspath=/home/user/pathtoNFS,nolock,rsize=1024,wsize=1024

    Use single quotes when you define bootargs so that the macros stay in place.  And use ip=dhcp so that the board will get its own IP address.

    setenv bootargs 'console=ttyS0,115200n8 noinitrd ip=dhcp root=/dev/nfs rw nfsroot=${serverip}:${nfspath} mem=128M'