This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF: LibFirstTimeConfig.a problem with iOS14

Part Number: CC3220SF


We are following below thread to use the update LibFirstTimeConfig.a to build the SimpleLink_WiFi_Provisioning_iOS_Source_2.2.26 sample app. 
The built app can't receive a confirmation from the device with iOS14, however it did work with iOS12. Is there an updated source code to fix this ?

https://e2e.ti.com/support/wireless-connectivity/wifi/f/968/t/784865?CC3220SF-SmartConfig-iOS-SDK-Missing-arm64-device-architecture-only-has-Simulator-architecture