Other Parts Discussed in Thread: MSP430F5529, , CC3100, CC31XXEMUBOOST, UNIFLASH
Hi guys, I'm struggling with setting up my CC3100BOOST with my MSP430F5529. I'm following the official guidelines but I'm stuck at point 5 of section 4.1. The device, in fact, doesn't appear in Windows10 device manager. As Figure 4 shows, there should be at least 2 ports belonging to CC3100, instead I only see the usual two of the underlying MSP430F5529 board. I know that "technically" the instructions are for CC31XXEMUBOOST, but it also says that it works just as well with any other MSP430 device.
I've already installed uniflash, the SDK and the drivers contained in the SDK folder but nothing... do you have any suggestion?
It may be that those ports shown in the Figure only shows for the CC31XXEMUBOOST, but then I wonder if I have to use the normal UART port I've always used for the MSP430F5529 or something else... there is no documentation on that.
Thank you
PS: the board works since I've tried it in Access Point mode and I could connect to it.