Other Parts Discussed in Thread: CC3100,
Hi team,
A customer is using CC3100MOD with the tcp_socket example, connecting multiple CC3100MOD to an H3C AP. As the number of station(CC3100MOD) increased, they found that the channel utilization of the AP increased significantly, leads to throughput decrease/dataloss eventually.
Below is the channel utilization diagram of the AP with 30 CC3100MODs connected. You can see ctlbusy is the total utilization and it's above 80%.
The customer also tested another wifi module(not TI product) and found the channel utilization is lower than CC3100MOD. Could you give some suggestions regarding to the use case of large network for CC3100MOD? What test could be implemented to find the cause of this? Any suggestion to decrease the channel utilization?
Thanks!
Best regards,
Shuyang