Hi,
In 3220 EVK, the SOP[1:0} = 001 or 010 are able to boot up without UART connected.
But it CC3220MODASM2MONR, we have 2 condition as below:
1. SOP[2:0] = 010, GPIO_01 & GPIO_02 need to connect to XDS110 debug probe's UART for booting, otherwise it wont boot.
2. SOP[2:0] = 001, it will be able to boot up whatever UART is connected or not.
We think that condition 1 will enter uart download mode without UART connected.
May I know what is the correct setting for SOP in CC3220MODA ? And relate HW schematic if have....
Thanks