Hi,
I have my WL1837MOD configured for 2x2 MIMO but when I connect to my AP, it only establishes an RX rate of MCS7 65Mbps. Shouldn't it have a higher rx bit rate for 2x2 MIMO?
Here are the commands I used
From swra489.pdf...
Mapping of ht_mode:
MIMO: use wl18xx.ht.mode=0
SISO40: use wl18xx.ht.mode=1 (default)
SISO20: use wl18xx.ht.mode=2
• Location of configuration bin file: /lib/firmware/ti-connectivity/wl18xx-conf.bin
root@am335x-evm:/usr/sbin/wlconf# ./wlconf -i /lib/firmware/ti-connectivity/wl18xx-conf.bin --get | egrep -i ht.mode
wl18xx.ht.mode = 0x00
root@am335x-evm:/usr/share/wl18xx# ./sta_start.sh
root@am335x-evm:/usr/share/wl18xx# Successfully initialized wpa_supplicant
root@am335x-evm:/usr/share/wl18xx# ./sta_connect-ex.sh bwc_comcast_24 WPA-PSK blablabla
netid=0
=========================
OK
OK
OK
OK
root@am335x-evm:/usr/share/wl18xx# wlan0: CTRL-EVENT-REGDOM-CHANGE init=BEACON_HINT type=UNKNOWN
wlan0: SME: Trying to authenticate with 9c:34:26:3b:a8:1e (SSID=[ 466.745126] wlan0: authenticate with 9c:34:26:3b:a8:1e
'bwc_comcast_24' freq=2462 MHz)
[ 466.763741] wlan0: send auth to 9c:34:26:3b:a8:1e (try 1/3)
[ 466.795355] wlan0: authenticated
wlan0: Trying to associate with 9c:34:26:3b:a8:1e (SSID='bwc_com[ 466.800478] wlan0: associate with 9c:34:26:3b:a8:1e (try 1/3)
cast_24' freq=2462 MHz)
[ 466.820860] wlan0: RX AssocResp from 9c:34:26:3b:a8:1e (capab=0x1431 status=0 aid=2)
[ 466.850151] wlan0: associated
wlan0: Associated with 9c:34:26:3b:a8:1e
wlan0: CTRL-EVENT-SUBNET-STATUS-UPDATE status=0
[ 466.935331] cryptd: max_cpu_qlen set to 1000
wlan0: WPA: Key negotiation completed with 9c:34:26:3b:a8:1e [PT[ 466.993707] IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
K=CCMP GTK=TKIP]
wlan0: CTRL-EVENT-CONNECTED - Connection to 9c:34:26:3b:a8:1e completed [id=0 id_str=]
[ 467.029035] wlcore: Association completed.
root@am335x-evm:/usr/share/wl18xx# iw dev wlan0 station dump
Station 9c:34:26:3b:a8:1e (on wlan0)
inactive time: 720 ms
rx bytes: 23538
rx packets: 84
tx bytes: 14311
tx packets: 76
tx retries: 0
tx failed: 0
beacon loss: 0
rx drop misc: 0
signal: -42 dBm
signal avg: -41 dBm
tx bitrate: 117.0 MBit/s MCS 14
rx bitrate: 65.0 MBit/s MCS 7
authorized: yes
authenticated: yes
associated: yes
preamble: long
WMM/WME: yes
MFP: no
TDLS peer: no
DTIM period: 1
beacon interval:100
short preamble: yes
short slot time:yes
connected time: 33 seconds