This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODASF: whether this WiFi chip support 802.11 k

Part Number: CC3235MODASF

Hello.

Whether this WiFi chip support 802.11k?

If not, do you have solution to support it?

What we are interested for 802.11k is mainly in roaming feature, so if this WiFi chip not support 802.11k, can it support roaming?

When CC3235 connect to AP1, and move from AP1 to AP2, the signal strength for AP1 is decrease and AP2 is increase. The CC3235 will disconnet first due to the signal strength is too weak of AP1, then start connect to AP2, or it can manage an auto switch connection from AP1 to AP2 without disconnect to the server? The "auto switch connection" is managed by CC3235 Network processor or need the user's appliaction to handle it?

Please detail about the threshold of "signal strength for AP1" and "signal strength for AP2" to trigger an "auto switch connection". How long will it take to complete the "auto switch connection"?