This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1831MOD: Tx Power over temperature range

Part Number: WL1831MOD


Hello,

The WL1831MOD datasheet gives a maximum Tx power of:

- WIFI : 17.3 dBm (Table 6-1, 1 Mbps DSSS)

- BlueTooth : 11.7 dBm (Table 6-2, GFSK).

Our understanding is that these figures apply to 25°C according to Chapter 5 preliminary note :

All specifications are measured at the module pins using the TI WL1835MODCOM8 evaluation board. All measurements are performed with VBAT = 3.7 V, VIO = 1.8 V, 25°C for typical values with matched RF antennas, unless otherwise indicated.

Could TI specify the WiFi & BlueTooth Tx power over the temperature range -20/+70°C ?

With many thanks in advance,

Best regards,

Thomas