Part Number: CC3135
Our customer refers
e2e.ti.com/.../boostxl-cc3135-firmware-update for their FW update procedure,
Then, they have some questions regarding the power loss while FW update process.
1. Is it possible to retry the update by the SPI between MCU and CC3135.
2. Is the first time like image writing required for this case by UART or SPI ?
3. Or Factory Rest is requried?
Also they would like to confirm thier following recognition. Please comment on these points.
(1) If the power is cut off during rewriting with sl_FsProgram, it will not be possible to recovered.
(2) When rewriting with sl_FsProgram, it is necessary to write the GangImage.
(3) If the power is cut off during rewriting with sl_FsWrite, Factory Reset is required to recover. # Even if the power is turned on normally, it cannot be started.
(4) sl_FsWrite is an API that rewrites only the service pack (sp_4.7.0.3_3.1.0.5_3.1.0.26.bin).
(5) At this time, the signature (sp_4.7.0.3_3.1.0.5_3.1.0.26.UCF.signed.bin) is also required.
(6) Service Pack and signature are handled as independent files.
(This means, There is no signed ServicePack.bin file)
Regards, A.Fujinaka