HI TI!
I am developing an application with the CC3220MODAS, the application must receive data via UART and send it via WIFI. Please, I would like to make sure that everything is ok and I am not missing some detail.
For the UART interface I have configured these pins: 42-UARTTX, 47-UARTRX, 51-UARTCTS, 52-UARTRTS.
At this point I have the following doubt:
How the chip (CC3220MODAS) knows that these pins are configured for UART functionality?
Do I have to do something to make the chip (CC3220MODAS) configure these pins with the respective UART functionality?
I have connected the pins VBAT_RESET to the 3.3V power supply and nRESET to the 3.3V power supply through a resistor pull up.
With these connections the module will be active and working?
The ANT_SEL1 and ANT_SEL2 pins are not connected.
With these connections will the wireless communication work?
Please could you explain me the functionality of the ANT_SEL1 and ANT_SEL2 pins?
I also have the RF_BG pin not connected.
I also have JTAG and SPi FLASH interface access connectors.
Please everything is ok, am I forgetting something?
Attached is an image with the wiring diagram of the connections.
Sincerely thank you very much!
Best Regards