This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC3235SF: ERROR: process command,-2050

Part Number: LAUNCHXL-CC3235SF

Dear TI,

I am running AT+Command example on LAUNCHXL-CC3235SF board and trying to connect to my network using the following command :

AT+WlanConnect="MyWiFi",,WPA_WPA2,"MyPassword",,,

I got the Error: process command, -2050 message. I don't know I got this SL_ERROR_WLAN_INVALID_ROLE.

Please clarify Slight smile

B R,

Brahim

  • Hi Brahim,

    The cause of this error is because your CC3235 is in AP mode. The CC3235 does not have dual role capability, so you can only be either a STA or an AP. Please switch to STA mode and retry your WlanConnect command like so:

    Fullscreen
    1
    2
    3
    AT+WlanSetMode = STA
    AT+Stop = 0
    AT+Start
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Regards,

    Michael