Part Number: CC3135MOD
Other Parts Discussed in Thread: CC3135, CC3220SF
I am using STM32 interfaced with TI CC3135 module for my application. I have ported the simplelink host driver to STM32 with FreeRTOS using the Host Driver Porting Guide in the document SWRU455M .
I have mapped all the asynchronous event handlers in the user.h file. The slcb_NetAppRequestHdlr is mapped to SimpleLinkNetAppRequestEventHandler.
I am using the latest SDK simplelink_sdk_wifi_plugin_4_20_00_10.
For provisioning, I start the NWP in AP mode and also start the internal HTTP server. I need to store the IP address of my server and so send a HTTP POST request with a custom token for it. I expect the SimpleLinkNetAppRequestEventHandler function to get called from which I can parse the required data but it doesnot happen. I am unable to trace the request in any of the event handlers.
All other events such as WLAN events, NETAPP events (for IP acquisition) work fine except for the NetAppRequest event.
Could you please guide me on how to solve this?