Hello,
Could you tell us the detail of the difference of the "Configuration" setting between MCU+Image and Debug on CC3220MODA?
You can see it on CCS project -> properties -> General -> Configuration.
We would like to know the following.
1.Is the "MCU+Image" setting prefered to build the project on this environment?
2.In case of "MCU+Image", does it read something information from the evaluation board and generate the code?
The background of this question is that it seems the build operation finish normally only when the "MCU+Image" setting.
Best Regards,
Nomo