This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF: ERROR: Cannot locate .sli image file.

Part Number: CC3220SF
Other Parts Discussed in Thread: SYSCONFIG

Hi all,

I am new to CCS and CC3220 so please bear with me.

I am getting:
ERROR: Cannot locate .sli image file.

when I try to Flash the program to launchpad. I can build the project and debug fine.

What can be the issue? I imported 'empty' example for TI-RTOS on CC3220 launchpad. Also, image.syscfg has an crossed line icon, what does that mean? Does that mean image is not ready?

Thanks,

Jay

  • Hi Jay,

    Note that CCS version 10.2 or newer is required to use all the features of SysConfig ImageCreator. Can you check your CCS version? What version of the CC32xx SDK are you using?

    If you are using the latest versions, please share a snippet of the icon. Does image.syscfg open? Also, please share the console output when you build the project.

    Best regards,

    Sarah