Other Parts Discussed in Thread: SYSCONFIG
Hello,
I configured the sysconfig like below.
And I set ip and NWP power like below when the module powered on. (My project based on the "at_commands" example)
Here are questions:
1. The MCU and NWP will enter to LPDS automatically if there are no actions. Is it right?
But the current consumption is about 18mA on my device after set the NWP power and no more action like above log. It seems that the MCU not entered to LPDS.
2. When I send AT Command like "at+wlanget=connection," after the MCU entered to LPDS, the MCU wakes up from LPDS ?
Or should I control the gpio 13 to wake it?
Thanks,
Calvin