Other Parts Discussed in Thread: UNIFLASH,
Hi,
I am not able to format CC3200 by using CCS uniflash. Attaching the schematic of CC3200 which i designed.
I found CC3200 is not able to generate following voltages-
- Voltage on VDD_ANA1 - which should be around 1.9V
- Voltage on VDD_DIG1 - which should be around 1.2V
- Even i am not getting any switching DCDC_PA_SW_P and DCDC_PA_SW_N.
- On further investigation i found Pin No. 38 (DCDC_ANA_SW) has very low impedance around 97ohm. Can i know the possible root cause of damaging of pin no. 38 pin?