Part Number: CC3220S-LAUNCHXL
Other Parts Discussed in Thread: CC3220S,
Hello,
I am currently working on a new design using the CC3220S.
One of the tasks I wish to implement is to measure sound volume levels of a single MEMS microphone.
The CC3220S datasheet documents there is a I2S peripheral interface,
and I was wondering if it can be used to interface with for instance a ICS-43434.
Which pins of the McASP/I2S pins should be connected ?
Are there some examples available ?
I also have a CC3220S-LAUNCHXL board which I would like use for testing...
Best regards,
Salvatore