Other Parts Discussed in Thread: TIDA-010022, CC1352R, , IWR6843, MMWAVEICBOOST, CC3235S, SYSCONFIG, LAUNCHXL-CC3235S
1. Please provide me source code of model in the document TIDA-010022 for demo, including device code and demo code on PC GUI via UART.
2. I see description of LAUNCHXL-CC1352R1 has wifi. But when I look at CC1352R MCU, it only has BLE, Multi-standard, Proprietary 2.4 GHz, Sub-1 GHz, Thread, Zigbee. Please confirm whether LAUNCHXL-CC1352R1 really has wifi and can connect via TCP/IP, UDP.
3. Which code in SDK simplelink_cc13x2_26x2 can I refer for CC1352 UART data reading from sensor?
4. Which communication protocol did you use for data transfer between 2 CC1352R1 modules? I think it's TCP/IP.
5. Which sample code can I refer for TCP/IP communication between 2 CC1352R1 modules? I can't find anything about it in SDK.
6. I see the reference design in document TIDA-010022 is sub-1 GHz type. What if I want to modify code for wifi communication? Which part do I need to modify?
I posted this thread in wifi forum even though the design in TIDA-010022 is for sub-1 GHz application because I'm trying to do a project via wifi. If it's more suitable to put this thread in sub-1 GHz 4rum, please help me transfer it to engineers on sub-1 GHz forum if you think this thread is more suitable on that forum. I expect engineers on both wifi & sub-1 GHz 4rum will help me on this issue.