Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: UNIFLASH, CC3220SF
Hi
1. Debug network_terminal project in CCS. It has uart log output. But when I reset the CC3220SF-launchpad or re-plug USB cable, there is no uart log output.
Is it programming to internal Flash or RAM?
2. I am writing SPI driver and refresh programming by CCS. It must to do re-plug USB cable operation before go full speed running in CCS. Otherwise, it stop at the code which I changed at this time.
3. If use Uniflash, does it programming image to external flash, or both external flash and internal flash? Thanks.