Other Parts Discussed in Thread: , CC2652R, CC2531, UNIFLASH, FLASH-PROGRAMMER
Hi,
I am running Zigbee Linux Sensor to Cloud demo on BB Black and CC1352P-2 LaunchPad.
After the building of the gateway completed, I tried to run the zigbeeHAgw script with a CC1352P LaunchPad as ZNP. The below error appeared and the gateway went into an endless loop trying to reset the ZNP.
Please find the log as below and please advice about this issue, thanks!
Best regards,
Shuyang
==========================================================
debian@beaglebone:~/source/Projects/node$ cd ~/source/out/Precompiled/servers
debian@beaglebone:~/source/out/Precompiled/servers$ sudo ./zigbeeHAgw
Platform type selected automatically as bbb.
To override this selection, please stop this script, and then run it again,
specifying the desired platform type at the command line:
./zigbeeHAgw [help | bbb | x86 ]
running ./zigbeeHAgw on an ARM
done processing arguments, board type bbb, target arm
NPI is 'NPI_lnx_arm_server'
Zstack linux server is 'ZLSZNP_arm'
gateway server is 'GATEWAY_SRVR_arm'
network manager is 'NWKMGR_SRVR_arm'
OTA server is 'OTA_SRVR_arm'
Starting the ZigBee gateway subsystem
making sure there are no lingering servers...
there are 0 NPI servers
there are 0 ZLS servers
there are 0 GATEWAY servers
there are 0 NWKMGR servers
there are 0 OTA servers
(total 0)
done
Executing reset from external scripts
===================================================
starting NPI, cmd ' ./NPI_lnx_arm_server NPI_Gateway.cfg -v 0x0000010E ' on Fri Jul 24 14:13:04 UTC 2020
[14:13:04.283,660] [NPISRVR/MAIN] UNMSKBL:
[14:13:04.284,076] [NPISRVR/MAIN] UNMSKBL: ************************************************
[14:13:04.284,105] [NPISRVR/MAIN] UNMSKBL: * NPI Server v1.0.2d *
[14:13:04.284,129] [NPISRVR/MAIN] UNMSKBL: ************************************************
[14:13:04.284,150] [NPISRVR/MAIN] UNMSKBL:
Startup phase 1 completed successfully, server started (NPI_PID=2501) on Fri Jul 24 14:13:09 UTC 2020
===================================================
starting ZLSZNP, cmd ' ./ZLSZNP_arm 127.0.0.1:2533 config.ini -v 0x0000460E ' on Fri Jul 24 14:13:09 UTC 2020
[14:13:09.650,350] [Z_STACK/MAIN] UNMSKBL:
[14:13:09.653,757] [Z_STACK/MAIN] UNMSKBL: ************************************************
[14:13:09.654,692] [Z_STACK/MAIN] UNMSKBL: * ZStack Server for ZNP v1.0.2d *
[14:13:09.655,316] [Z_STACK/MAIN] UNMSKBL: ************************************************
[14:13:09.657,964] [Z_STACK/MAIN] UNMSKBL:
[14:13:09.658,986] [Z_STACK/MAIN] PKTTYPE: [ NPISRVR<<Z_STACK ] [AREQ] 08:5F:00:02:5A:5F:53:54:41:43:4B
[14:13:09.660,325] [NPISRVR/MAIN] PKT_HEX: New incoming connection from client Z_STACK (connection # 5)
[14:13:09.662,238] [Z_STACK/MAIN] PKTTYPE: [ NPISRVR<<Z_STACK ] [SREQ] 02:25:3E:FF:FF
[14:13:09.664,614] [NPISRVR/MAIN] PKT_HEX: [SOCZIGB<<NPISRVR ] [send] 02:25:3E:FF:FF
ERR:: Input/output error
[ERR] npi_ipc_errno 0x02030100
Exit socket while loop
[14:13:11.674,503] [Z_STACK/MAIN] ERROR : SRSP Cond Wait timed out!
[14:13:11.674,924] [Z_STACK/MAIN] ERROR : apicSendSynchData() failed getting response
[14:13:11.675,082] [Z_STACK/MAIN] PKTTYPE: [ NPISRVR<<Z_STACK ] [SREQ] 01:2F:09:00
[14:13:13.675,885] [Z_STACK/MAIN] ERROR : SRSP Cond Wait timed out!
[14:13:13.676,292] [Z_STACK/MAIN] ERROR : apicSendSynchData() failed getting response
[14:13:13.676,441] [Z_STACK/MAIN] PKTTYPE: [ NPISRVR<<Z_STACK ] [SREQ] 01:2F:06:00
Startup phase 2 failed
NPI_lnx_arm_server: no process found
waiting for NPI to exit
making sure there are no lingering servers...
there are 0 NPI servers
there are 0 ZLS servers
there are 0 GATEWAY servers
there are 0 NWKMGR servers
there are 0 OTA servers
(total 0)
done
Executing reset from external scripts
===================================================