This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
During the RF test based on one of our CC2652P module, we found a problem
Hardware: RF-star RF-DG-52PA based on CC2652P
Test software: RFStudio 7
Test conditions: ZigBee protocol, TX power: 20 dBm, Center Frequency: 2480 MHz
When RBW is 1 MHz, there is a -30 dBm spurious emissions at the frequency of 2430 MHz. The reference photos are as follows:
We are applying for the certification, this problem is found. Hope you can help us to solve this problem and we can get the certification ASAP.
Thanks a lot.
Sunny
Hi,
Did you check on our CC1352P-2 Launchpad?
Does the Spur level changes with the Tx Power Level? Just reduce the Tx power (for example 17dBm) and check the Spur level again.
I observed you are using older version of SmarRF Studio. Could you please update to the latest version and test again?
We can help you in reviewing your design and see any issues related to your design.
You can request the Design Review by using the following link. You need not upload the files with the Request. Just 1st send the request then the concerned engineer will reach out to you and request for files.
Thanks,
PM
Hi PM,
Thanks for your reply.
Actually, the spurious emission is always existing, no mater what tx power we set. We had tried all the TX power level.
We will update our design in the link you gave me.
Hope this problem can be solved ASAP.
Thanks & Best regards.
Sunny
Hi Sunny,
As we are going to use the other link for Hardware design review then I want to close this post.
Thanks,
PM
Hi Sunny,
I already provided a link in my 1st reply. The following is the link again for your ready reference.
Thanks,
PM