I've been developing my ZigBee application with a couple of CC2530EMs (which use CC2530f256 chips) and have them working just fine. Then we designed a couple of new modules with CC2530f128 chips, and we seem to be having problems, but I can't tell if it is related to the chip change or maybe something else. The bug that we run in to when trying to run our application on the new modules is that when trying to set the device type using the zb_WriteConfiguration function, the NV memory seems to never be set. Is this related to the difference in chip? Or is there some other reason that zb_WriteConfiguration might not work?
Matt