Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352P: Non functional after unboxing; missing components on pcb

Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: CC1352P, FLASHTOOL, UNIFLASH,

After unboxing a brand new dev board with LOT no: 3072018LK3, the CC1352P seem to not work.

Tests performed so far:

- Attach via USB to PC -> OK, both XDS ports are detected

- Program hex via XDS with TI Flashtool (UniFlash & TI RF-Programmer tested) -> OK, hex could be written and verified

No program execution visible with no precompiled hex, nor own hex-files.

Performed visual inspection of assembled pcb -> NOK at least C461 & C471 (7.5pF 0201) are missing

Hand soldering of new C461 & C471 8pF 0402 -> measurement OK but No program execution visible

Crystal startup is visible

What else can be done and which other problems are known with this lot no?

Regards,

Andreas