Part Number: CC2531
Hi , may you all give me a hand? I tried to connect the CC2531 on a YOCTO 2.0 OS,
when I run ~lsusb , I can see that recognice the USB port:
root@Docsis-Gateway:/# lsusb
Bus 004 Device 010: ID 0451:16a8 Texas Instruments, Inc.
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
but when I go to /dev I can not find the ttyACM0, also, I got same issue on a Alpine 3.12
my question is: doesnt linux recognize automatically the drivers? or I need to do something else to my linux/Yocto to got the ttyACM0 ?
thank you for help me
BR