Other Parts Discussed in Thread: SYSCONFIG, CC1352P, TIMAC
Hi,
I'm trying to rename the Application Name in Sysconfig of a project based on simplelink_cc13x2_26x2_sdk_5_10_00_48's zr_sampleapp. However, the generated zclConfigInit function in zcl_config.h still has references to sampleApp_serviceTaskId inside the #ifdef BDB_REPORTING block. Changing C:\ti\simplelink_cc13x2_26x2_sdk_5_10_00_48\source\ti\zstack\.meta\templates\zcl_config.c.xdt, lines 436 and 567 to
bdbString += '\tZstackapi_bdbRepAddAttrCfgRecordDefaultToListReq(' + appNameCamel + '_serviceTaskId,&Req);\n';
seems to fix it.
Also, I found that the Application dir is missing from the compiler includes.
I missed something when I imported the project?
Thanks,
Robson