This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: Unable to pair devices

Part Number: CC2652P
Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1, UNIFLASH, CC2531, CC2530, CC2652R

Hi Team,

Recently I purchased CC2652-LAUNCHXL board, and I am trying to compile a ZNP firmware from it. I installed CCS 10.3.0.00007 and used Simplelink SDK 5.10, I could successfully build the ZNP from the example and the Z-tool is connecting to the LAUNCHXL, but when I try to pair any Zigbee devices it is not pairing. Moreover where could I find the Coordinator.js file for CC2652. I build the default example without any changes made. Please help us to resolve this. Thanks