Part Number: CC2652P
Hi,
can CC2652P support the 1.8V regulated mode? thanks.
BR. Albin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Albin,
Are you asking whether the CC2652P can be run with an external regulator? If that is your question, then I believe that should be fine, but I don't believe you'll be able to get 20 dBm of output power in that configuration because that requires VDDS to be your bias voltage in the RF circuitry. In the datasheet, the TX output power numbers are generated with VDDS = 3.0V. You should be able to get the 10 dBm path though, which is biased with 1.8 V of VDDR.
Best,
Nate