This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: Can RTC keep value after system reset?

Part Number: CC2652P

Hi, I use CC2652P, simplelink_cc13x2_26x2_sdk_4_40_04_04, my application is based on sensor 2.4G example as below:

Now, I can use AONRTCCurrent64BitValueGet to get RTC value.

When system reset, the rtc value will be reset and start from 0 again.

My question is, is there any way to keep RTC value continuing running after system reset, so that after system reset, the rtc value I get is not reset to 0?

For example, when sometime RTC value is 1000, and system reset at this time, after system reset, rtc value continues running from 1000.

Can I achieve this? Thank you.