Part Number: CC2652R
Dear all,
We have built a ZNP using CC2652, and we are using Zigbee lighting ON-OFF and Dimmer modules with it, we are using ZDO_BIND_REQUEST function to get the manual switch feedback. After binding I am getting the feedback properly for ON-OFF switches in AF_INCOMING_MSG format, But for Dimmers I am getting the button press status in AF_INCOMING_MSG format but the the data is not exact for ON and OFF status.
I am getting the below message for ON-OFF button press from Dimmer modules, for both ON and OFF the message is same.
<RX>06:24:28.37 COM5 AF_INCOMING_MSG (0x4481)
GroupID: 0x0000
ClusterID: 0x0008
SrcAddr: 0xAC11
SrcEndpoint: 0x01
DstEndpoint: 0x07
WasBroadcast: 0x00
LinkQuality: 0x81
SecurityUse: 0x00
Timestamp: 0x001A9727
TransSeqNumber: 0x00
Len: 0x07
Data: .I... @ (0x08, 0x49, 0x0A, 0x00, 0x00, 0x20, 0x40)
I am getting the same message for ON as well as OFF. Kindly help me to get the exact status.