This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Implementing a new clusterin SE profile.

Other Parts Discussed in Thread: CC2530

Hi,

I have a requirement of implementing a new cluster which has different attributes than of Simple metering. I am using CC2530 chip with Zstack. It has around 104 attributes. The problems i am facing are

 

1). When I tried to run both the clusters together ..i am recieving XDATA not enough error. So i had to disable the  simple metering cluster. Is there a way to run both simultanously using semaphores?? I think it has only 8k ram...104 attributes has a total size of around 4000 bytes. is it possible to run this cluster??..

2) I tried to implement my own commands , similar to sm_getprofilecmd for data collection. But i am not able to receive the command in Rx side. i am using zcl_sencommand to send..but the receiving handler is not getting the command it seems.

Then i tried using the zcl commands like zcl_sendread() & zcl_Inprocesscmd() for the Tx & Rx of the attributes. I am getting some data in debug string returned from rx.     Which one is better making using own command or zcl_senread??

3) can any value be given for  new cluster ID?

4) The receiving buffer size is limited to 128 bytes..is it possible to extend it???

Awaiting a speedy response..

Shree