Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: CC2652P: MODULE DOES NOT RUN AFTER RESTART.

Part Number: CC2652P
Other Parts Discussed in Thread: CC1352P, UNIFLASH, Z-STACK

Hello,

SDK 5.10

device: BDE RFM-207P

I am working on BDE-RFM207P. The chip consists the module of cc2652p. i am facing the problem related to the program starts after reset. please find the below steps which I am doing.

1. Program using cc1352P board to the module.

2. The example is zr light.

3. I am referring the sdk 5.20 latest and the cc1352P-2 example from RTOS.

4. when I have flashed code into device its works fine.

5. but after that i have  just do the power cycle of the module. after that it will not work.

Please guide me.

  • Hello Chintamani,

    Are you saying that the device works well in a CCS/IAR debug session but cannot recover from a power cycle afterwards?  Is the same true if the project's output hex file is programmed using Uniflash or Flash Programmer 2?  How do you verify that the device is not operating as expected?  Have you followed all instructions from the BDE-RFM207P USER GUIDE?  Keep in mind that this document has instructions for a BLE project which do not apply to Z-Stack, for example defining CUI_DISABLE and/or removing BOARD_DISPLAY_USE_UART would be used in place of Display_DISABLE_ALL.  Since these examples work well on TI LaunchPads, you should consider contacting BDE for further suggestions/assistance with their module.  Linked is the BDE-RFM207P Datasheet with contact information.

    Regards,
    Ryan