Other Parts Discussed in Thread: CC2530
Hi,
In "CC2530_ZNP_Schematic.pdf" document, 11 pins are needed to connect between MCU and CC2530.
CC2530_DC
CC2530_DD
MRDY
SRDY
CFG0
CFG1
SO
SI
CC2530_SS
CLK
CC2530_RESET
But, I'm not sure that which pins are essential or can be hard wired.
For example, CFG0, CFG1 are not used in sample code. In CC2480 datasheet, the pins are for the type of communications.
Also, it seems MRDY and CC2530_SS can be hard wired to GND.
And, if CC2530_DC and CC2530_DD pins need only for programming, I think, it doesn't need to connect also. Right?
Could I have any information for minimum pin connection beetween MCU and CC2530 on final product design?
Thank you.
J.J