This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HUE Philips lamp connected to ZNP but is not present in Associated List Devices

Other Parts Discussed in Thread: CC1352P

I use CC1352P in ZNP mode and ZTool.

HUE Philips lamp was paired to the ZNP with APP_CNF_BDB_START_COMMISSIONING command.

ZDO_ACTIVE_EP_REQ command works, I see the lamp c lusters.

I can send AF_DATA_REQUEST command to send on/off and it works.

But when I send command UTIL_GET_DEVICE_INFO, the lamp is not present in the AssiocDevicesList.

<RX>10:40:18.27 COM10 UTIL_GET_DEVICE_INFO_RESPONSE (0x6700)
    Status: SUCCESS (0x0)
    IEEEAddr: 0x00124B001CA1BC04
    ShortAddress: 0x0000
    DeviceType: COORDINATOR (0x1)
    DeviceState: DEV_ZB_COORD (0x9)
    NumAssocDevices: 0x00
    AssocDevicesList

UTIL_ASSOC_COUNT returns 0 of associated devices.

<TX>10:43:26.69 COM10 UTIL_ASSOC_COUNT (0x2748)
    StartRelation: 0x00
    EndRelation: 0x00

<RX>10:43:26.69 COM10 UTIL_ASSOC_COUNT_RESPONSE (0x6748)
    Count: 0x0000

But when I send command UTIL_ASSOC_FIND_DEVICE, I get the response with short address of the lamp.

<TX>10:44:04.99 COM10 UTIL_ASSOC_FIND_DEVICE (0x2749)
    Number: 0x00

<RX>10:44:05 COM10 UTIL_ASSOC_FIND_DEVICE_RESPONSE (0x6749)
    Device: o_........c....... (0x6F, 0x5F, 0x00, 0x00, 0x04, 0x08, 0x00, 0x00, 0x00, 0x01, 0x63, 0x00, 0x00, 0x00, 0x1D, 0x00, 0xFF, 0xFF)

0x5F6F is the short address of the lamp.

Why the lamp is not in the associated list? What is wrong?