Hi,
I use:
board: Launchpad-CC1352R
SDK: 5_10
I have a simple program based on the PinStandby example from TIREX.
There is only one change. Two lines inside the main thread that are responsible for LED toggling have been removed.
I use this program to check energy trace for the simplest scenario, transition STANDBY->ACTIVE->STANDBY.
When I set standbyDuration to 1000ms, I see the following energy trace:
There are two main parts: red and blue.
The red part is a recharge pulse, and the blue is the actual transition.
In this case (period=1000ms), I can see one additional "standalone" recharge pulse between adjacent wakeups.
Everything is as expected. The energy of the recharge pulse depends on the time since the last recharge and so on.
Unfortunately, when I set standbyDuration to 100ms, I see the following energy trace:
There are three main parts: red, blue, and extra yellow.
What is this yellow part for?
Regards
Adam