This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: Battery Charger and CC1352 battery monitoring

Part Number: CC1352R
Other Parts Discussed in Thread: BQ21040, Z-STACK,

Hi 

I am designing kind of a ZigBee button that would be powered by single coin cell. For battery level monitoring I want to use MCU internal temperature and battery monitor functions. But also I will be charging the battery by BQ21040. 

When I check the maximum battery monitor range, it is 3.8V. Battery charging voltage is 4.2V. 

What is the best and cheapest way to protect MCU while charging and using battery monitoring function?

Best regards,