Other Parts Discussed in Thread: CC1352P, CC2538
Hello Community,
I am working on the CC238 & CC1352P Zigbee devices.
Our end devices have energy monitoring functionality with an auto-calibration feature. (i.e measuring & reporting the parameters associated with Voltage, Current & Power for load/appliance)
I have read the ZCL Specification document & found that the following sections are useful to full fill our requirements.
Chapter 3: section 3.3 Power Configuration
Chapter 4: measurement & sensing
Chapter 10: Smart Energy
Chapter 15: Appliance
But I would like to add 2 additional functionality.
1. Start & Stop Calibration.
2. Detect the Load/Appliance connected to the Zigbee device (CC2538/CC1352) or Set the Connected Load/Appliance.
I would like to go with the Zigbee standards to implement the functionality mentioned above.
I am looking for the above configuration in the ZCL Specification Document, but am unable to find any source related to it.
Will you please help me to know,
1. How can I map calibration & load detection functionality to cluster & which is the suitable or recommended cluster for it.
Regards,
Shiv Patil.