Part Number: CC1352R
Other Parts Discussed in Thread: SYSCONFIG
SDK 4.40.0.44
2x Launchpads cc1352r1
1st LP - "dmm_zed_switch_remote_display_app" project
2nd LP - Smart RF Studio connected
We want to implement the tests in the CUI menu, but when we call the command HCI_EXT_ModemTestTxCmd(LL_EXT_TX_MODULATED_CARRIER, 0), nothing happens. We don't see any signal on another LP board with Smart Rf Studio. We selected the channel 37 (2402MHz) in the SmartRf studio.
We also tried HCI_EXT_EnhancedModemTestTxCmd(LL_EXT_TX_MODULATED_CARRIER, LL_EXT_RF_SETUP_1M_PHY, 0), the same result.
All these functions return success result (0).
We added the parameter -DHCI_TL_FULL in the "build_component.opts" otherwise it got stuck in rom_init.c ROM_Spinlock().
We tested both launchpads with Smart RF studio in TX -> RX mode, both works fine. We saw signal.
How could we start the test? Could it be that we don't initialize something and that is why the test doesn't start?
P.S. In our old BLE project based on SDK 3.10.00.53 the test was working well without any issues, although it had -DHCI_TL_NONE in the "build_component.opts" file.