Part Number: CC2530
Other Parts Discussed in Thread: CC2592,
What's the occupied bandwidth(OBW) of CC2530+CC2592 in TX mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The 99% BW is about 3.5MHz at max TX power.
Becomes smaller at lower power levels.
Also refer to this app note:
https://www.ti.com/lit/an/swra465a/swra465a.pdf
regards
Thanks.
So, OBW will be 2MHz to 3.5MHz when TX power from min to max value?
Well, typical testing equipment,like IQ2010 or CMW500,their OWB for Zigbee is 2MHz. How to use those device to test TX power from CC2530+CC2592?
Hi,
I think CMW500 might have a spectrum analyzer mode which you can use the measure the BW. See the user manual.
regards