Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: Z-STACK
Good evening (o;
As a new user getting his feet wet on the cc13x2-26x2 SDK.....which supports the dmm feature...
Is this only used when I want to use ZigBee and BLE concurrently on a ZNP or also for the 868MHz radio built-in?
Reason for asking:
Development of a ZigBee gateway with dual ethernet and wifi....and as we have still a big stock of legacy room thermostats in the 868 range running a 802.15.4 MiWi protocol a cc1352 device would be a perfect match....so we could have a smooth migration moving from MiWi to ZigBee 3.0. Not sure yet if BLE is needed in the deployment scenario.
thanks in advance
richard