Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
Issue:
The customer distinguishes different domains by modifying the parameters of DEFAULT_TC_LINK_KEY, and the nodes are modified. However, the actual operation of two domain networks is still free to group, and it is not possible to separate the two networks.
The customer would like to know is there any other way to achieve it.
The original contents of the nwk_globals.h file are as follows:
// ZigBee Alliance Pre-configured TC Link Key - 'ZigBeeAlliance09'
#define DEFAULT_TC_LINK_KEY { 0x5a, 0x69, 0x67, 0x42, 0x65, 0x65, 0x41, 0x6c,\
0x6c, 0x69, 0x61, 0x6e, 0x63, 0x65, 0x30, 0x39 }
The modified contents of the nwk_globals.h file are as follows:
// ZigBee Alliance Pre-configured TC Link Key - 'ZigBeeAlliance09'
#define DEFAULT_TC_LINK_KEY { 0x20, 0x69, 0x67, 0x42, 0x65, 0x65, 0x41, 0x6c,\
0x6c, 0x69, 0x61, 0x6e, 0x63, 0x65, 0x30, 0x20 }
Thanks!
Best Regards,
Cherry Zhou