This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: Problem with firmware upload.

Part Number: CC2652R
Other Parts Discussed in Thread: UNIFLASH

Hello,

We've designed our pcb based on CC2652R MCU.
Now we want to program it (as programmer we are using that one placed on CC26x2 LAUNCHPAD XL) and have some strange issue.

What exactly happens:

- For the first time upload of the firmware was success - program boots and run as expected.

- For the second time upload failed and IDE showed  this error:

- Then if i upload firmware again, upload succeed but program doesn't boot.

Then i tried to use UniFlash tool. So i tried to upload firmware again and got this error:

But if i do whole flash memory clear before programming, then firmware uploads and runs as expected.

I've no idea what can cause this issue. We've tried three pcbs and one works well always, and on the other two we've this problem.

Additional info.

We've tried also another CC26x2 LAUNCHPAD as programmer, but nothing changed.

We tried to upload some examples from SDK to exclude that our firmware causes this issue, but the same occurs.

Version of CCS i'm using: 10.4.0.00006

Version of UniFlash: 6.4.0.3394

SDK Version: SimpleLink_CC13x2_26x2_4.30.00.54

Best regards,

mf