Part Number: CC2652P
Other Parts Discussed in Thread: SYSCONFIG, Z-STACK
Hello,
I've been using the examples in the Resource Explorer for the CC2652R1 and CC1352P1 evaluation boards but I want to start customizing the code. There's no exact example for what I need. I just need a basic Zigbee project for 802.15.4-2006 using 250kps with no operating system, no Z-stuff or anything like that. I want to evaluate receiving and sending packets. I've been looking at others who ask this question on the forum, but I can't seem to figure something out. I'm not sure where they pulled the code changes from.
I've taken projects like rfEchoTX and rfPacketTX and played with SysConfig to change the RF type from the proprietary type to 802.15.4. That obviously doesn't change any of the source code such as what is found in the mainthread() so the build immediately fails. My question is how do I pop new code in there that supports all the libraries so that it makes those demos work again with the new RF protocol? I wish there was a demo project that had this functionality instead of jumping into the network topology as soon as the demos try to use the 802.15.4 protocol. It seems like there is a bit of a gap in the examples, but maybe not. Could you help point me in the right direction and how to get a basic example like this going so that I can build up from there?
Thank you!
Michael