Other Parts Discussed in Thread: Z-STACK, CC1352P, CC2652P
Hi,
I've bought a CC2562R SonOff dongle and it works just fine with ZigBee2MQTT, but since I have to write a Java Z-Stack implementation I was testing some command. (see title for firmware version)
The dongle answer correctly to all the command I've so far tested, but when it comes to ZB_WRITE_CONFIGURATION (code = 0x2605) instead of answering me with 0x6605 it gives me with 0x6000 ( which consulting the Z-Stack Monitor and Test API doesn't seem to exist)
I've used a serial port sniffer to check the results.
[02/12/2021 12:30:24] Read data (COM3)
00 .
[02/12/2021 12:30:25] Read data (COM3)
fe 06 41 80 00 02 01 02 07 01 c0 þ.A€......À
[02/12/2021 12:30:25] Written data (COM3)
fe 00 21 01 20 þ.!.
[02/12/2021 12:30:25] Read data (COM3)
fe 02 61 01 59 06 3d þ.a.Y.=
[02/12/2021 12:30:25] Written data (COM3)
fe 00 21 02 23 þ.!.#
[02/12/2021 12:30:25] Read data (COM3)
fe 0a 61 02 02 01 02 07 01 14 64 34 01 00 2b þ.a.......d4..+
[02/12/2021 12:30:25] Written data (COM3)
fe 00 27 00 27 þ.'.'
[02/12/2021 12:30:25] Read data (COM3)
fe 0e 67 00 00 17 76 c2 24 00 4b 12 00 fe ff 07 þ.g...vÂ$.K..þÿ.
00 00 b1 00 ..±.
[02/12/2021 12:30:28] Read data (COM3)
fe 06 41 80 00 02 01 02 07 01 c0 þ.A€......À
HERE IS THE PROBLEM (read data is dongle's response)
[02/12/2021 12:32:05] Written data (COM3)
fe 03 26 05 03 01 03 21 þ.&....!
[02/12/2021 12:32:05] Read data (COM3)
fe 03 60 00 01 26 05 41 þ.`..&.A