Part Number: CC2520
Hello TI Friends & Family,
Interesting question regarding available cc2520 package/part numbers.
Per the below Table in the Package section of the DS, what are the different part numbers and what do they mean?

This is interesting – as it appears there is no other online collateral related other than the device datasheet.
Quickly, I can tell unequivocally that all four (4) part numbers are pin-compatible. IN fact, there is only 1 package type offered for this cc2520 device…the “VQFN RHD 28” as defined in the Package section of the DS.
The “R” in the part number suffix (last character) means Reel, as in packaged on a Reel in 3000 pcs quantities.
The “T” in the part number suffix (last character) means Tape/Tray, as in packaged on a Tape/Tray in smaller 250 pcs quantities.
The “HPAxxxx” part appears to be a custom part number version of the same base cc2520 but would need to confirm.
The “G4” suffix also is unknown; would need to confirm.
Any further input/clarification would be helpful!
TY,
CY