Other Parts Discussed in Thread: UNIFLASH, CC2531EMK, CC2652P
Hi,
I've recently bought a XDS110 and it finally arrived.
I have a sonoff dongle CC2652 that due to some firmware update I cannot connect it to USB anymore so I decided to connect via CJTAG and erase it.
I connected it (XDS110) to my pc and it automatically downloaded the drivers.
I connected the 20-to-14 JTAG to CTJAG adapter and connected the pins to my Sonoff CC2562P dongle ( check below for dongle's pin layout )
Opened FLASH PROGRAMMER 2 to mass erase my CC2562P but it says device may not be in bootloader mode.
Do I have to do something to setup my debug probe before using it? Or I can run it like that?
PIN CONNECTION I MADE:
14 ADAPTER DONGLE
5 vcc
8 GND
1 tms
11 tck
2 rst
SONOFF LAYOUT PIN