This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: For Static IPV6 for nodes

Part Number: CC2652R

Hello,  Am new to thread Protocol  and i have 3  launchpads of CC2652R1 .

Tested CLI FTD and Temperature code works well , But it i do network reset in any node through cli  and again it connects to leader as child , IP address changed .

So is their any way or option for static IP for nodes ?

  • Hi,

    This should be the expected behavior.

    One place to explore might be the openthread configurations related to address assignment (e.g. see OPENTHREAD_CONFIG_IP6_SLAAC_ENABLE, OPENTHREAD_CONFIG_DHCP6_CLIENT_ENABLE).

    Happy holidays and new year!
    -Toby